2004-08-05 1:44 AM
2004-08-04 2:38 AM
I am having a problem using the InDart-STX and the ST7FLITE09.
When I press f5 the code runs when I press Shift f5 the code should just stop, in my case the code stop but the ST7 resets and the program counter jumps to the start. I use the Indart with another ST (ST7F324) device with no problems i.e. when you press shift f5 the code stops Wherever it was & the micro does not reset. I have the options set to ''No Reset in Halt'' Any clues on what I am doing wrong Regards, Brian2004-08-04 11:19 AM
This is standard behaviour for the FLITE0x range.
This is mentioned in page11 of the Softec STX User’s Manual Addendum. ''Note (ST7FLITE0-specific): when in real-time emulation, the “Stop Program� command causes a chip reset.'' Regards sjo2004-08-04 8:38 PM
Thanks for the info, I always forget about the addendum which is larger than the main manual! I looked on the their website but could not find anything.
Is there a get around so that I can pause the code to see what the registers are doing? Re Brian[ This message was edited by: BrianM on 05-08-2004 11:14 ]2004-08-05 1:44 AM
Not really, you could use a trap instruction to stop the core without a reset.
Regards sjoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.