2019-10-15 5:55 AM
Hi,
I was thinking of developing a small project using ST8 processors, but I did not find information on what do I start from.
The link https://www.st.com/en/microcontrollers-microprocessors/stm8-8-bit-mcus.html#
lists commercial compilers. Are there free compilers for ST8, same as for STM32?
Thank you,
Solved! Go to Solution.
2019-10-21 6:52 AM
Hello
First thing is your MCU selection. It is going to depend on the nature of your project
Automotive (STM8AF/AL)- NonAutomotive (STM8S/L)
Mainstream or Low power (STM8S or STM8L)
Then I suggest you to start with STM8CubeMX and select the appropriate P/N, and configure the device according to your needs.
Several IDE are available (depending on your preference), offering Free C compilers
https://www.st.com/en/microcontrollers-microprocessors/stm8s-series.html#tools-software
Ordering the 64pin Nucleo for the Hardware is a good start as it comes with different exemples. it is a quick hands-on solution.
https://www.st.com/en/microcontrollers-microprocessors/stm8s-series.html#tools-software
For programming the STlink-V3 will be useful for STM8 and STM32.
I hope this will help you to initiate your development.
Kind regards
2019-10-15 7:33 AM
If you mean STM8 MCU then Yes. It is SDCC with GDB. https://stm8-binutils-gdb.sourceforge.io/ This is C only compiler by GNU public license.
2019-10-21 6:52 AM
Hello
First thing is your MCU selection. It is going to depend on the nature of your project
Automotive (STM8AF/AL)- NonAutomotive (STM8S/L)
Mainstream or Low power (STM8S or STM8L)
Then I suggest you to start with STM8CubeMX and select the appropriate P/N, and configure the device according to your needs.
Several IDE are available (depending on your preference), offering Free C compilers
https://www.st.com/en/microcontrollers-microprocessors/stm8s-series.html#tools-software
Ordering the 64pin Nucleo for the Hardware is a good start as it comes with different exemples. it is a quick hands-on solution.
https://www.st.com/en/microcontrollers-microprocessors/stm8s-series.html#tools-software
For programming the STlink-V3 will be useful for STM8 and STM32.
I hope this will help you to initiate your development.
Kind regards
2019-10-22 7:37 AM
You can get the IDE: ST Visual Develop for free from ST.
I use it with the (free) compiler: CSSTM8 from Cosmic.
You need to register your pc (via email, their webinterface doesn't work) to get a license.
This license is for one year, but after that you can simply ask for another license.
Also download the Standard Peripheral Library from ST.
I use partly this library, partly I do direct register configuration.
Succes,
Wilko
2019-10-22 7:41 AM
The ST-Link V2 works fine as well.
About STM8CubeMX, is it still under active development or is it abandoned? And will errors (see other posts here) in the Standard Peripheral Library be fixed?
Wilko
2019-10-30 8:57 AM
@AlexFjedoseev @Community member Ake and I have implemented link-time unused code elimination and better GNU binutils support for SDCC. Thanks to these modifications, SDCC can now be considered a serious alternative to propietary compilers such as CXSTM8 or IAR.
See the following link for a small working code example showing these new features:
https://github.com/XaviDCR92/stm8-dce-example
STM8 port of GNU binutils:
https://github.com/XaviDCR92/stm8-binutils-gdb
Fork of SDCC featuring GNU assembler support and bugfixes:
https://github.com/XaviDCR92/sdcc-gas
Also, build OpenOCD 0.10 for ST-Linkv2 support:
https://sourceforge.net/projects/openocd/files/openocd/0.10.0/openocd-0.10.0.tar.bz2/download
2019-11-08 4:37 AM
For a large number of evaluation boards,
http://www.colecovision.eu/stm8/
has tutorials for getting started using hte free tools (i.e. the Small Device C Compiler and stm8flash).
2019-11-18 7:24 AM
Thank you, Wilko
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.