soft reset for stm8s003f3
hi,i am developing a code, i want to soft reset the micro using instructions in cosmic C compiler. can any one help?
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
hi,i am developing a code, i want to soft reset the micro using instructions in cosmic C compiler. can any one help?
Hi All,This is my first post here and also my first interaction with ST micro devicesI'm truing to flash a .hex file into an STM8S103F3 using ST LINK V2 and STVP but I cannot connect to the device. I'm using a 5V external supply connected to the VDD ...
Hello,Could you please send me all below details for ST25R3920B-AQWT ? Rev. of AEC-QHTOLTemp.-GradeHTOLTest-temperatureHTOLTest-durationSelf-heating Driving ChargingPrecondit-ioningOn-Grid ParkingOff-Grid Parking
Good morning, I should reprogram a "SPEAr1310" do you have any device that does this?Thank you.
Pl suggest the Maximum Junction temperature of ST33KTPM2X32CKE3 and ThetaJa (k/W)
Hi,I have a custom PCB with STUSB4500 as the UCPD controller and STM32H7 as my application processor. Without any I2C communication between stm32h7 and stusb4500 the stusb4500 is able to negotiate a higher voltage from a usbC PD source by matching it...
Where can I buy this IC? I can't find any information for it. If it is obsolete can you point me to the datasheet and alternatives?
Please I have mini board with processor STM8S103F3 and I need use I2C communication for OLED 128x32 panel SSD1306. Is there examples for ARDUINO IDE or STV Developer and Cosmic.Thank you very muchZdenek
Hi! i have two stm8105c6t6 , i want use one to master and other to slave, two pcb board are connect using 10k pull up resistor in the SDA/SCL line. i am using the example AN3281 stm, but my microcontroller not have tim4, i change the tim4 to tim3 bu...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.