2019-07-05 4:40 AM
I configure the portB 4,5,6,7 as external interrupt pins. the program is working well if any interrupt occurs in portb 4,5,6,7 the execution send to irq. how to find which pin irq is occured in portb
please give the solution to my problem
2019-07-05 7:59 AM
look for PR bits in EXTI block.
They are set when the defined edge(s) occur.
Clear the PR bits after reading them.
2019-07-07 9:40 AM
What I do, is store a variable with the current status of the pins. In the interrupt I just read the current port values and compare it with the known status to see what pin has toggled.
You need to pay attention on how your system is setup. It also depends how the sensitivity bits are configured for the 4 pins.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.