2009-03-09 3:11 AM
2011-05-17 12:58 AM
Hi all,
We have a 4mb (256k x 16) SRAM connected to the EMI as 16bit at CS0, we can read & write up to A15, but writes to A16-A17 do not work, although we can see activity on A16-A17, we are unsure if this is at the correct time. Any Ideas?? Here is the setup: /* GPIO7 Configuration */ GPIO_DeInit(GPIO7); GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2; GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull; GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt2 ; GPIO_Init (GPIO7, &GPIO_InitStructure); /* GPIO0 Configuration CS0 & 1 & 2*/ GPIO_DeInit(GPIO0); GPIO_InitStructure.GPIO_Direction = GPIO_PinOutput; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_6; GPIO_InitStructure.GPIO_Type = GPIO_Type_PushPull; GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt2; GPIO_Init (GPIO0, &GPIO_InitStructure); /***** EMI Setup *****/ /* Enable the clock for EMI*/ SCU_AHBPeriphClockConfig(__EMI | __EMI_MEM_CLK, ENABLE); SCU_AHBPeriphReset(__EMI | __EMI_MEM_CLK,DISABLE); /*BCLK=96Mhz*/ SCU_EMIBCLKDivisorConfig(SCU_EMIBCLK_Div1); /*Enable the Mux mode*/ SCU_EMIModeConfig(SCU_EMI_MUX); /*ALE length and polarity definition*/ SCU_EMIALEConfig(SCU_EMIALE_LEN1, SCU_EMIALE_POLHigh); /* EMI Address/Data GPIO Setup */ GPIO_EMIConfig(ENABLE); /* EMI default configuration : Reset configuration*/ EMI_DeInit(); //Bank 0 CS0 EMI_StructInit(&EMI_InitStruct); /* Number of bus turnaround cycles added between read and write accesses.*/ EMI_InitStruct.EMI_Bank_IDCY = 0x3; /* Number of wait states for read accesses*/ EMI_InitStruct.EMI_Bank_WSTRD = 0x1f; /* Number of wait states for write accesses*/ EMI_InitStruct.EMI_Bank_WSTWR = 0x1f; /*Output enable assertion delay from chip select assertion*/ EMI_InitStruct.EMI_Bank_WSTROEN = 0x3; /*Write enable assertion delay from chip select assertion*/ EMI_InitStruct.EMI_Bank_WSTWEN = 0x3; /*This member Controls the memory width*/ EMI_InitStruct.EMI_Bank_MemWidth = EMI_Width_HalfWord; /*Write protection feature */ EMI_InitStruct.EMI_Bank_WriteProtection = EMI_Bank_NonWriteProtect; /*Use Bank0 (CS0)*/ EMI_Init( EMI_Bank0, &EMI_InitStruct);We’re moving the ST Community to a new platform to give you a better and more reliable community experience.