2009-03-09 10:57 PM
STR912 UART2 - No RX IRQ after 1 byte (FIFO disabled)
2011-05-17 12:58 AM
Hi Everybody!
I cannot reach receiver IRQ on UART2 (STR912FAW44 rev.H) after one byte! I have configured UART with FIFO disabled. Everything works fine when the received answers are longer than 1 byte. But when answer is one byte long, the STR912 UART2 does not generate RX IRQ. I need interrupt after each byte to service STM32 Cortex boot loader protocol, that (unfortunately) gives such (1 byte length) results, ex. 0x79 or 0x1F. Earlier i have done receiving in polling (works OK), but now i want to have IRQ. Can someone help me ?? P.S. STR912 Documentation is - like always - completely poor...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.