2023-05-03 5:28 AM
Hi,
I'm using the latest EEPRMA2 drivers for the M95M04 EEPROM.
I'm trying to store data in EEPROM on a specific address.
In the following example, I expect one byte to be written to address 5.
uint8_t a = 10;
uint32_t targetAddr = 5;
EEPRMA2_M95_WriteData(EEPRMA2_M95M04_0, &a, targetAddr , sizeof(a));
Stepping into EEPRMA2_M95_WriteData, we go into M95_spi_WriteData which still has the size of 1, but moving to the step where EEPRMA2_SPI_SendBuffer is called, the size has changed to 6 bytes to be written. It looks like the size is defined from the remainder, which is based on the following equation: ( targetAddress + Size ) % PageSize
I don't see how this can be correct implementation?
Edit: I seems like this person has the same problem https://github.com/STMicroelectronics/X-CUBE-EEPRMA1/issues/4
2024-03-14 3:25 AM
int32_t M95_spi_WriteData(M95_Object_t *pObj, uint8_t * pData, const uint32_t TarAddr ,
const uint16_t PageSize, const uint16_t Size )
{
int32_t status = M95_OK;
uint32_t targetAddress = TarAddr;
uint16_t remainingSize = Size;
// Calculate the starting page and offset
uint16_t startOffset = TarAddr % PageSize;
uint16_t offset = startOffset;
// Check for invalid inputs
if (pObj == NULL || pData == NULL || PageSize == 0 || remainingSize == 0) {
return M95_ERROR; // Return an error code indicating invalid inputs
}
if (pObj->IO.IsReady( pObj->IO.Address ) !=M95_OK)
{
return M95_ERROR;
}
// Iterate over the pages and write the data
while (remainingSize > 0)
{
uint16_t bytesToWrite = (remainingSize < PageSize - offset) ? remainingSize : (PageSize - offset);
/* Condition Matters only for 4Kb SPI ie M95040, for others EEPROMEX_WRITE & EEPROMEX_UPWRITE are same */
if (pObj->IO.Address == 0xC6)
{
if (targetAddress < 256)
{
status = pObj->IO.WriteBuffer( pData, targetAddress, pObj->IO.Address, bytesToWrite ,EEPROMEX_WRITE);
}
else
{
status = pObj->IO.WriteBuffer( pData, targetAddress, pObj->IO.Address, bytesToWrite ,EEPROMEX_UPWRITE);
}
}
else
{
status = pObj->IO.WriteBuffer( pData, targetAddress, pObj->IO.Address, bytesToWrite ,EEPROMEX_WRITE);
}
pObj->IO.Delay(6);
// Update the pointers and sizes for the next page
pData += bytesToWrite;
targetAddress += bytesToWrite;
remainingSize -= bytesToWrite;
offset = targetAddress % PageSize;
// Wait for the SPI interface to be ready before proceeding to the next page
while( pObj->IO.IsReady( pObj->IO.Address ) != M95_OK ) {};
}
return status;
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.