2024-11-26 6:34 PM - last edited on 2024-11-27 6:06 AM by Andrew Neil
This is one of function in code to implement WS2812 LED protocol on STM8S003F3.
And I am getting this error compilation.
----------- Project ws2812_led - STM8 Cosmic - Configuration Debug -------------
Compiling main.c...
cxstm8 -i..\led_blink\inc +debug -pxp -no -l +mods0 -pp -i"C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Hstm8" -clDebug\ -coDebug\ main.c
#error cpstm8 main.c:34(9+7) invalid typedef usage
#error cpstm8 main.c:34(24) i undefined
main.c:
The command: "cxstm8 -i..\led_blink\inc +debug -pxp -no -l +mods0 -pp -i"C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Hstm8" -clDebug\ -coDebug\ main.c " has failed, the returned value is: 1
exit code=1.
main.o - 4 error(s), 0 warning(s)
What could be the reason as I am using right data type?
Regarding WS2812 addressable LED strip with STM8S003F3, Is there any library like FastLED is available for STM8? If not then is there any other way, because I am facing difficulties while achieving nano sec delay for this protocol.
2024-11-27 6:02 AM - edited 2024-11-27 6:09 AM
As far as I remember, COSMIC does't accept variable declaration inside loops. Replace it for something like:
void ws2812_send_byte(uint8_t byte){
uint8_t i=0;
for(i=0;i<8;i++))
{
...
}
}
You can try to port FastLED to STM8
https://github.com/FastLED/FastLED/blob/master/PORTING.md
Googling around I've found this https://github.com/thielj/FastLED-STM8 but there's no documentation regarding the port, except reading the commits. Looks abandoned, but maybe it's a start point.
Good luck!
Regards
2024-11-27 6:17 AM
@gabs wrote:As far as I remember, COSMIC does't accept variable declaration inside loops.
The option of a declaration was added in C99: https://en.cppreference.com/w/c/language/for
@vatsal_1770 so the question is, what C specification(s) does your compiler support?
Their documentation just says, "This implementation conforms with the ANSI and ISO Standard C specifications" - which is very vague.
https://www.cosmicsoftware.com/stm8.php
https://www.cosmicsoftware.com/pdf/cxstm8_pd.pdf
"ANSI C" is usually taken to mean C89 - which certainly doesn't support the variable declaraion within the for.
2024-11-27 6:36 AM
Use older C styles, where variables are defined as you open scope, ie '{'
For nano-second times, perhaps use the TIM, more directly/explicitly to drive PWM, or patterns for modulation.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.