2024-11-30 9:47 AM - last edited on 2024-11-30 11:47 AM by Peter BENSCH
Hello,
I'm looking to read and write on an stm8s105K6c6 of a hoover, and would like any information that would enable me to carry out these tasks (chip and st-link v2 wiring diagrams), as well as the most appropriate software...
Thank you
*This post has been translated from French to comply with the ST Community guidelines.
2024-11-30 2:03 PM
Welcome @mbr972, to the community!
I would be very surprised if the manufacturer of the hoover had not protected the IP of the STM8 with the ROP function (see data sheet, section 4.4). I am therefore not holding out any hope that you will be able to realise your project successfully.
Regards
/Peter
2024-11-30 11:05 PM - edited 2024-11-30 11:30 PM
Merci, je suis novice en la matière. Et veux tenter l'expérience, j'ai acheté une stm8s105k6t6, mais je ne sais pas les correspondances entre le st-link et la puce, du moins pas de certitude.
RST= NRST pin 1
SWIN= PD1 SWIN pin 42
SWCLK= PD0 pin 41
SWDIO= VDDIO_1 pin 8
3.3v = VDD pin 7
GND= VDDA pin 13
Merci cordialement
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.