2023-09-20 1:54 AM
Hello,
I am trying to start a new project on a STM8s003K3 discovery kit, i have downloaded and installed STVD without a problem but I can't download Cosmic C Compiler. The download link in the Cosmic site is not working, I have tried anything I can think of (changing DNS settings, resetting IP, checking host file) to fix timeout error thinking the problem was on my end but I can't download it on another pc connected to another WiFi either so I think it is the download link which is broken. Any ideas what might be the issue? If this is unfixable there any other opensource compiler for stm8s?
Solved! Go to Solution.
2023-09-20 4:24 AM
Yes, I did test it with another browser, it is still the same. It seems like the problem is my location afterall.
Thank you again for your fast replies.
Best regards,
Enis
2023-09-20 3:11 AM
Well, I just checked it again - works fine. You just have to enter your data on this website and then you will be redirected to the website with the actual and current download (Windows EXE, about 24MB).
Hope that helps?
Regards
/Peter
2023-09-20 3:30 AM
Thank you for your response, I tried the link you provided but again I got "ERR_CONNECTION_TIMED_OUT" error. If it's working fine for you, can there be a problem about the region I am at? I can't really think of anything else.
Sicerely,
Enis
2023-09-20 4:01 AM
Have you ever tested another browser?
Otherwise, it must have something to do with your location or IP and access seems to be blocked somewhere along the route. Unfortunately, this cannot be determined from the outside, but you can check the route with tools like tracert.
Good luck!
/Peter
2023-09-20 4:24 AM
Yes, I did test it with another browser, it is still the same. It seems like the problem is my location afterall.
Thank you again for your fast replies.
Best regards,
Enis
2023-09-20 4:32 AM
OK, if the problem is solved, although perhaps not to your complete satisfaction, please click Accept as Solution. This will help other users find that answer faster.
BTW: you can always post a solution to your problem here in the thread later if you have found it, other users with the same problem would certainly be pleased.
Regards
/Peter
2025-05-08 3:29 AM
I also encountered the same error. When I click on the register and download link on the Cosmic C Comiper website, I get an error. Did you fix this error that you encountered, how did you fix it?
Best regards,
Enes
2025-12-15 11:52 PM
Using a FOSS toolchain to target the STM8, will avoid all the hassle of registration and licensing. SDCC is an excellent FOSS compiler targeting the STM8.
However, unlike the non-free compilers it doesn't come with an IDE; many SDCC users use SDCC together with a third-party IDE, such as Code::Blocks or Visual Studio.
2025-12-18 6:30 AM
2025-12-22 12:36 AM
Thank you for your response and the detailed explanation.
I followed the steps you suggested and was able to resolve the issue.
Best regards,
Enes
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.