2006-08-03 5:52 AM
Code & Block Protection command in ST10flasher.dll
2006-08-03 5:52 AM
Hello all,
In our company production is carried out by external company which include st10f269 programming. To avoid misuse of hex file we develope one tool using STflasher.dll which accept Encrypted file and Decrypted internaly and use same to program the chip. But st10flasher.dll wont have Code and Block protection command,so it is possible for someone to read our code using ST10 flasher. if it is possible for ST Microelectronic to provide Code and Block protect command in ST10flasher.dll then it is real helpfull to us as our tool (using st10flasher.dll) will direct execute protection command after programming and will avoid MISUSE OF HEX FILE. if someone having different solution to our problem then please help. regards... YogeshWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.