2006-08-03 12:42 AM
2006-08-02 10:32 PM
hi
I'm working on a debug interface for ARM7 and I'm facing a problem I have to stop the program running on the CPU using EMbeddedICE. In order to do that, I'm choosing scan chain 2, which is the one for EmbeddedICE then, I need to scan the data in this scan chain. The data should be bit 1 high, all the other bits low address 00000 to reach the debug control register bit for read/write high however, while executing that, the program keep on running is there someone who can give me a hand? :-[2006-08-03 12:42 AM
Have you looked at Openocd, could save you a lot of code/time.
http://openocd.berlios.de - i have just added support for the str9 which will be added to svn soon. Regards sjoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.