Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Replacement part for M24M01-DFCS6TP/K

M24M01 parts, other than the wafer option, are currently NRND. We have a design that uses an M24M02 and want to add two M24M01s on the same bus. Is there a pin compatible replacement for this part with the same configurable I2C address capability, or...

krmayer by Associate
  • 1032 Views
  • 1 replies
  • 0 kudos

L9966 Resistance measurement overall accuracy

hello, L9966 datasheet (§8.2) mentions a max total resistance measurement accuracy of 1.5% (if CALIB_SEL=1). It seems that such accuracy does not include external pull up RRx accuracy which should impact the overall measurement accuracy and therefore...

DavidL by Associate
  • 1262 Views
  • 1 replies
  • 0 kudos

Resolved! STW81200 Custom Library

Hello Everyone,Can anyone help me out !Currently, I am working with STW81200 RF Synthesizer Module by using the STM32 Controller. I have used STW81200GUI Tool for frequency generation. But I don't want to use the tool anymore. I want to write my own ...

How to write M95256 flash memory

Hello,       I'm using M95256 IC as the external EEPROM for the controller.  When I test the write flash memory operation, I found that the memory could not write yet, my instrcution order shows below:       step 1: read status register       step 2:...

yangma_0-1726627029076.png
yangma by Associate
  • 1458 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.