Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Help identifying this component 211

I can't find reference to this component, I'm trying to repair/understand the equipment.  Does anyone recognize this part? Secondly, I couldn't find any reference on the ST website about component identification markings.  A link or reference would b...

Galvin by Associate
  • 1728 Views
  • 1 replies
  • 2 kudos

Transient period over current problem.

A 24 VDC, 10 A AC/DC converter design has been done using the eDesignSuite on the ST website. The converter gives a very stable output at 24 VDC. We did not encounter any problems when we used the converter at normal loads below 10 A. However, when w...

sonerA by Associate
  • 2433 Views
  • 2 replies
  • 0 kudos

a LOT of problems with KEIL uVision

Hello. I am a very beginner in STM32 and in electronics overall and I have a really big issue with Keil uVision5. I was following my tutorial, the guy in the video told me to create a project in CubeMX and then generate code and open in in Keil uVisi...

Снимок экрана 2024-10-23 213112.png Снимок экрана 2024-10-23 213120.png Снимок экрана 2024-10-23 213125.png Снимок экрана 2024-10-23 213147.png
EhoMen by Associate
  • 3651 Views
  • 1 replies
  • 0 kudos

Sainsmart STM-5045 Stepper Driver repair?

I have two Sainsmart STM-5045 4.5a stepper drivers that i would like to get running, i had a pretty tough day last week with my machine and had to put this aside for a bit but i would like to see if i can salvage either of them today.The order of eve...

frank22 by Associate
  • 1354 Views
  • 1 replies
  • 0 kudos

Blue Pill: No STM32 Target Found

  im using STM32F103C8T6 , Im using it without any problem but yesterday i upload code , the code is not correct then i make some changes and upload again then it showing this error i use both ST-LINK UTILITY and STM32CubeProgrammer , i follow some s...

mubarak_0-1729675848217.png mubarak_2-1729676325521.png mubarak_3-1729676354416.png
mubarak by Associate II
  • 3383 Views
  • 7 replies
  • 3 kudos

Resolved! Setting 3.3V on STEVAL-USBI2CFT Adapter

Hello,I'm trying to set the voltage to 3.3V on my STEVAL-USBI2CFT adapter, but I'm unclear on how to do this. The user manual (UM3226) mentions setting the voltage via soldering jumper JP4. However, my board has seven solid pads labeled J8, J4, J5, J...

geometer by Associate II
  • 2873 Views
  • 4 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.