Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

EEPROM ST 950406 replacement

Hi,any help or information to find the data sheet and to determine an available replacement type for an obsolete EEPROM chip from ST marked 950406 would be highly appreciated.A picture of the chip is attached.The defective EEPROM chip 950406 comes fr...

Tom6 by Associate
  • 2519 Views
  • 2 replies
  • 1 kudos

Looking for USB type C PD controller IC

Hi,I'm looking for  USB type C PD controller IC.We need 3 USB type C ports in our design. 1st port should support dedicated power in (up to 140W) and the 2nd and 3rd port should be dedicated for power out (65W) with variable power outThe product oper...

PY.1 by Associate II
  • 1703 Views
  • 2 replies
  • 0 kudos

Resolved! M24C01/M24C02 device addressing restriction

Hi,We're developing a PCB that can have multiple different I2C ICs assembled and have chosen the M24C02-RMC6TG EEPROM for board identification.In the datasheet, section 4.5, a note states no other device using the 1010 xxxx address can be connected t...

STM-EEPROM.jpg
LazarCG by Associate II
  • 3039 Views
  • 5 replies
  • 5 kudos

mmWave radar solution for UAV detection

Hi, expertsI want to use mmWave radar soc suggested by ST to do the UAV detection. The equipment is located on the ground.Not sure any solution from ST for UAV detection is available?Can ST give a solution to satisfy the requirements below ?My requir...

Resolved! Pocket size of taping

Hi, members.Would you please let me know the package details for USBLC6-4SC6?I need to know the tape dimensions for width(A0) and length(B0) and thickness(K0).   Thank you.Best regards,

smallfumiki_0-1730102534988.png

Issue with MCP4541-104E/MS digital pot

I recently created a digital potentiometer breakout board for the MCP4541-104E/MS, where I would set the resistance value dependent on a particular wiper value. Here is the schematic and layout (I changed the pullups from 10k to 4.7k):  Here is the c...

DRicc2_0-1730053887909.png DRicc2_1-1730053911904.png DRicc2_2-1730054219730.png
DRicc.2 by Senior
  • 1237 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.