Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STUSB4700 - constant output switching

We are using the STUSB4700 in our PD implementation as a source. We have encountered an issue where it seems like the output is constantly switched on/off/on/off with about 500ms on, 200ms off timing.Below is the schematic which connects to a USB typ...

AlexandrG_0-1729577539449.png AlexandrG_4-1729578119498.png
AlexandrG by Associate II
  • 2867 Views
  • 5 replies
  • 0 kudos

emmc card not detected

Actually I’m interfacing emmc . when I 'm working with sd card it detects sd card , but when comes to emmc it doesn’t detects emmc card , so how to solve these issues and how to power up this emmc module and emmc doesn’t have card detect pin, so how ...

sai1 by Associate II
  • 1439 Views
  • 1 replies
  • 0 kudos

Usage of BAL-NRF01D3 with AD8341

Good morning,In a university project we are using an nRF24L01 chip to produce a signal, which is then split and modulated by means of other devices.The final stage of each of the split signals is a AD8341 chips which has a 50ohms differential output....

Saitama by Associate
  • 893 Views
  • 0 replies
  • 0 kudos

Resolved! Where can I get the "X-Cube-WiFi1 expansion software package for STM32Cube" for the WiFi modules IDW01M1 and IDW04A1?

I want to use the WiFi module IDW01M1 and/or IDW04A1. In both quick-Start-Guides I get the tip to download the "X-Cube-WiFi1 expansion software package for STM32Cube". Unfortunately all the Links for this file are broken/dead.Is this package compatib...

CSeid.1 by Associate II
  • 5234 Views
  • 5 replies
  • 1 kudos

Resolved! 2N2907AHR Spice Model

Good Morning,I downloaded the zip file for the 2N2907AHR SPICE model, but Windows complains that the folder is empty and cannot be extracted. Can someone else confirm this behavior, and if so would it be possible to post a working copy?Thank you,Jon

Firmware Problem

Hello,I am somewhat new to the STM environment, but I started because I have a project where I need to implement CAN, and I happened to come across an STM8 discovery kit. This comes with an ST-Link integrated with an STM32, but I have tried to progra...

imagen_2024-10-18_013749809.png 5f45be28-5999-4340-a83f-73addd443a55.png
KalebG13 by Associate
  • 1419 Views
  • 2 replies
  • 2 kudos

Resolved! BSET BRES with dynamic position

Hello, I'm successfully using BSET and BRES assembler instructions where the position is constant. However, I'm having trouble getting it to work where the position is determined at runtime.For example: bset 0x500f, 2 ; works ldw x, (0x03, sp) bset 0...

Resolved! HAL_Delay is not working properly for stm32 blue pill

i'm trying to run a simple blinking led program on my stm32f103c8t6 (after i run it several times before successfully), and it doesn't work, when i fix the delay in 1000 ms the led is always on, when i decrement it to 100, 200, 300 it's working prope...

Monssef_0-1729150589677.png Monssef_1-1729150612727.png
Monssef by Associate II
  • 4067 Views
  • 8 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.