Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

EK302DL

Posted on January 03, 2012 at 21:20Hi, I can start EK302DL but I cannot run it under WIN7/64.  Is it necessary to useit only within WIN XP ?  I tried three different PCs with WIN7, every time EK302DLenters a endless loop. Parameters seem to be ok. ...

STVD V4.3.0 Hangs on Edit

Posted on December 16, 2011 at 09:33Hi, My setup : Windows Vista STVD V4.3.0 Cosmic C compiler STM8S Discovery board I use the example project 'stm8s-discovery_led'. I have opened the '\Project\Discover\STVD\Cosmic\Discover.stw' workspace and it bui...

joost by Associate
  • 1551 Views
  • 3 replies
  • 0 kudos

SSP problem

Posted on December 22, 2011 at 07:08I used the SSP sample code and enable SSP0 without loopback. I still get the transmitted dummy data when I send it for receving. After I test the sample code,I found that the GPIO setting cause this effect. I used...

kawumwx by Associate
  • 905 Views
  • 0 replies
  • 0 kudos

stm8s003k3

Posted on December 14, 2011 at 11:48i want to configure uart of stm8s003k3  as i have the code of uart for stm8s105c6t6 chip but when i select the stm8s003k3 chip complication  gives and error.can anyone please tell me what can i do for same code to...

IEC60730-Class C- RAM structure

Posted on December 03, 2011 at 07:59HiThis is ehsan, student of milan university, I am doing my final project in university which is relates to implementing Class c of IEC 60730. One of the routines which should be implemented, is RAM test routine v...

STVD 4.3.0 crash

Posted on November 30, 2011 at 21:51Hello,I have a problem with STVD 4.3.0. When I try to open the workspace the program crash. Behaves the same way when I create a new project and trying to modify it in the editor. The problem appeared only in vers...

Linker problem ''symbol d_imul not defined''

Posted on November 04, 2011 at 01:51I'm building a project for an STM8S208 using the Cosmic compiler (CXSTM8_32K) within ST Visual Develop.  When I link, I receive the error ''symbol d_imul not defined''.  The project was working well previously usi...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.