2011-12-16 12:33 AM
Hi,
My setup : Windows Vista STVD V4.3.0 Cosmic C compiler STM8S Discovery board I use the example project 'stm8s-discovery_led'. I have opened the '\Project\Discover\STVD\Cosmic\Discover.stw' workspace and it builds fine - no errors. Whenever I try to open a source file (e.g. main.c), STVD shows the hourglass and freezes. No editor window opens, no source file is shown. The source file path that STVD shows is OK. What am I doing wrong ? #stvd2011-12-18 1:08 PM
Hi , i think logging in as an administrator may solve your problem because i was having the similar kind of problem with my STVD and it was solved by logging in as administrator. (use the default administrator user)
2011-12-29 9:26 AM
Hi,
I've done the install on a new PC(also Vista, no other available) and I have exactly the same problems : when trying to edit a file, STVD hangs... It also does that when breaking in the debugger : I open the basic Discover project, send it to the debugger (without trying to edit anything). I can start the program (F5). When I then hit shift-F5 (stop and break), STVD tries to open the source file where it stopped and hangs... I've tried every Windows trick I know (run as admin, run in XP compatibility mode, use short path names without spaces, ...) without any change. This is a very consistent bug and can not be that hard to find. TOO BAD THERE IS NO RESPONSE FROM ST ON THIS - ABANDONING THIS MICRO - SORRY ST. JGW.2011-12-29 11:55 AM
I've the similar issue after upgrading to 4.3:
https://my.st.com/public/STe2ecommunities/mcu/Lists/STM8SDiscovery/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fSTM8SDiscovery%2fSTVD%204.3%20crashes%20on%20while%20editing%20projects%20from%204.2&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000CCDF802E596CAF44ADED5E61F5C... You can download latest 4.2.x -- it works. I hope that after Christmas and New Year we will have an update for the IDE...We’re moving the ST Community to a new platform to give you a better and more reliable community experience.