2012-01-02 6:28 AM
Hi All,
Since I accidently changed my system clock to a time in the future and set it back correctly, I get an error when ST Visual Development (using Cosmic in the backgrounds) compiles. It's an license-error more specific: FlexIm error: -88 ''System clock has been set back''So that, this message is appearing
&sharperror cpstm8 C:\Program Files\COSMIC\CXSTM8_32K\Hstm8\modsl.h:1 FlexLM System clock has been set back.
The error is known by COSMIC, I got this information: ''FLEXlm checks the computer for files with a timestamp beyond the current date. If there are files with a creation date in the future of what the current system clock reads, FLEXlm will return this error. These files must have been created when the clock was set incorrectly.
As a result of re-installing Cosmic-32k I was hoping that the problem could go away but still the problem occurs..
I would appreciate If any of you is able to help me to solve this issue..Regards, #flexlm-system-clock-has-been-setWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.