Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Counter TIM4

Posted on February 13, 2012 at 16:01Hi! I have a probem with a simple software that I've wrote to learn to use timers.This is the code that I've used.&sharpinclude ''stm8l15x.h''main(){   TIM4_DeInit(); TIM4_TimeBaseInit(TIM4_Prescaler_2048, 200); T...

karl246 by Associate
  • 1560 Views
  • 2 replies
  • 0 kudos

STVD 4.3.1 : swim error [30103]

Posted on February 09, 2012 at 11:57Hi, I'm running windows 7 64 bit, my target is STM8S103F2U. STVD gives me this error when trying to debug: ''failed to download application: error: swim error [30103]: rlink communication error''.    Rlink does no...

STM8S003F3 & GPIOA

Posted on January 19, 2012 at 10:27Hello.I am new for this CPU. I use the discovery board to test my SW.I use 3 pin on GPIOA pin 1 2 and 3:GPIO_Init(THRUSTER_STATE, BOW_STATE , GPIO_MODE_IN_PU_IT); // PullUp input with interruptGPIO_Init(THRUSTER_ST...

How to identify the reset source

Posted on January 04, 2012 at 10:12I use ST7MC1K2B6 to control a BLDC motor with sensorless . when I boost voltage to 200V, MCU is reset. I don't use LVD and WDG, I just use a POR(Power On Reset,20k/10uF). I change the RC parameter, but improvement ...

Hello world example

Posted on December 30, 2011 at 16:00 Hi there ! I am a newbiein ST microcontroller. 1) Tobeginning, I bought : * A http://www.st.com/internet/evalboard/product/251jsp (with a stm8l101K3 MCU) * A http://www.raison...

gege089 by Associate
  • 1724 Views
  • 2 replies
  • 0 kudos

stvd ver 4.3.0 not open file of project

Posted on January 05, 2012 at 18:31regards to all. I have installed stvd ver 4.3.0 and free cosmic C compiler,the problem is that  i can notopen anyfiles of the project to edit,the IDE hangs with lost functionality. There is a solution to this probl...

STM8L-Discovery Debugging

Posted on January 21, 2011 at 08:27Hello, I use the ST Visual Develop IDE together with the Cosmic Compiler and the STM8L-Discovery. Everything seems to work fine, besides the debug function. When I try to start debugging I get the following error m...

stm8 by Associate II
  • 6786 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.