Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cosmic 32K compiler for STM8

Posted on February 04, 2014 at 14:31My STM8 Cosmic compiler (32K limited) does not work anymore because it seems that the free licence is out of date (but it isn't: it will run out August 2014). Compiler Error is: '' </p>   #error cpstm8 C:\Programm...

IAR Kickstart STM8L05 EEPROM

Posted on February 04, 2014 at 11:50Hi I'm using the 8K limited IAR Kickstart compiler on the STM8L051F3 (8K) I'm using EEPROM and get the following 3 Linker errors Error[Li005]: no definition for ''__eeprom_program_byte'' [referenced from eeprom_ut...

Andre1 by Associate II
  • 2930 Views
  • 5 replies
  • 0 kudos

UNABLE TO MODIFY EEPROM

Posted on February 03, 2014 at 12:57Hello,I am having issues writing data into EEPROM of Stm8s003K3. I am using Stm8s Discovery development board and IAR IDE.I know the algorithm of unlocking the eeprom.I have attached the code I am using. The probl...

What is u16/u8 etc?

Posted on January 25, 2014 at 20:48I am reading it in help files, variables declared as u16/u8 etc. What is this? Does it meanu16=unsigned int typeu8=unsigned char type ?

singhd3 by Associate II
  • 3631 Views
  • 1 replies
  • 0 kudos

Can STM8S be used with an low cost RF receiver?

Posted on January 30, 2014 at 01:05Can STM8S be used with an low cost RF receiver, like the ones available on ebay for $1-$2? If yes then can someone help me identifying library/functions to execute this task. Thanks #interfacing-anything-to-anyt...

singhd3 by Associate II
  • 1337 Views
  • 1 replies
  • 0 kudos

ST7 SPI and JTAG Debugger working together

Posted on January 29, 2014 at 09:20I need to implement SPI communication on ST7. However the same IOs(Clock and data) used also for Jtag Debugger communication. Will the debugger will work correctly. i use the Cosmic compiler with Raisonance Rlink J...

Functions and parameters Cosmic C problem

Posted on January 27, 2014 at 19:32I am new to programming in C after years of using Basic on PICs. I would like to know where should I look for functions associated with a peripherals like GPIO ADC etc and what parameters they can accept. I am usin...

singhd3 by Associate II
  • 1191 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.