2007-09-17 2:10 AM
System crashes when initialize FMI (FMICLK = RCLK/2 )
2011-05-17 12:46 AM
Hi all...
I write a bootloader, it occupies at bank1, takes application from uart and write bank0.I wrote problems to forum on various stages.Anyway I encounter a new problem. When i was bank1, tried to write to bank0.But my application crashed. First i did SCU_AHBPeriphClockConfig(__FMI, ENABLE); SCU_AHBPeriphReset(__FMI, DISABLE); and in the startup.s FMICLK = RCLK/2 If i enable fmi clk and disable reset application doesn't run? What can i do for this problem. Regards... Mehmet2014-02-11 11:30 PM
Same issue I am facing, with PLL and RCLK set to 96MHz and FMICLK configured to 48MHZ (RCLK/2), I see the microcontroller crashing and gets hanged up. I could bring it back to life only after a System Reset/Power Cycle.
Microcontroller used : STR912FAW46x6.Crystal : 12MHzWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.