cancel
Showing results for 
Search instead for 
Did you mean: 

What is u16/u8 etc?

singhd3
Associate II
Posted on January 25, 2014 at 20:48

I am reading it in help files, variables declared as u16/u8 etc. What is this? Does it mean

u16=unsigned int type

u8=unsigned char type ?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Andrew Neil
Super User
Posted on February 02, 2014 at 23:11

The trouble with int, char, etc is that the 'C' language does not specify what size these types are - they are implementation defined.

That's why people create ''custom'' types of explicitly-defined size & signedness:

u16 - an unsinged 16-bit value;

s8 - a signed 8-bit value;

etc, etc,...

http://c-faq.com/decl/int16.html

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.