Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TIM1 TRGO FOR ADC

Posted on October 26, 2014 at 15:40I work on ST-Microcontroller  :STM8S003F3U6.I try to use TIM1 as a trigger (TRGO) for ADC interrupt.When I use the single pulse (TIM1_CR1_OPM=1)   mode (on TIM1 counter overflow) everything seems to work well, but ...

nataliap by Associate
  • 761 Views
  • 0 replies
  • 0 kudos

STLUX 385 - GPIO interrupt.

Posted on October 21, 2014 at 11:25Hi, I have problem with gpio interrupt. I am trying configure and enable interrupt by calling function GPIO_Init(GPIO0, GPIO_PIN_0, GPIO_MODE_IN_FL_IT) but without success. In interrupt handler function INTERRUPT_H...

Secure Debug Authentication

Posted on October 17, 2014 at 15:19I am using SPEAr1310 (SPEAR1310CPUC evaluation board, revision 1). I want to use Memory Mapped debug interface to setup breakpoints. I have read the interface base address using cp14 Cooprocessor (DBGDRAR, DBGDSAR)...

vln by Associate
  • 913 Views
  • 0 replies
  • 0 kudos

STR9 - Inrush current on the VDD supply

Posted on July 29, 2014 at 16:52Hi, I have a issue with the power supplies of my electronic board at start up of microcontroller STR912FAW47. Someone know the inrush current of microcontroller on VDD (1,8V) and VDDQ (3.3V) at power on? With an oscil...

jtual by Associate II
  • 1460 Views
  • 2 replies
  • 0 kudos

Bootloader not responding

Posted on October 04, 2014 at 12:31I'm using STM8L151G6 in a device. I've erased program and data memory using STVP and set bootloader checks 1 and 2 in option bytes (although as i understand this is not necessary since there is no data at address 0...

0690X00000602m2QAA.jpg
dscdsc by Senior
  • 1223 Views
  • 1 replies
  • 0 kudos

pointer problem (sdcc assembler)

Posted on September 26, 2014 at 16:37HelloWith the code below, i get returned an incremented caracter it self , the pointer is not,is it normal ? meaning my code is wrong . i mean i get U not O ...Or should I file a bug at sdcc comunity? ldw X,&shar...

remi2 by Associate II
  • 4421 Views
  • 12 replies
  • 0 kudos

GPIO pin not driven high

Posted on September 04, 2014 at 14:58Hello, Ich have a question. I am connecting the output pin (PC7) of STM8S003K3 to input pin (PC7) of STM8S207S. When I set the pin to high, I do not see the input pin PC7 (as interrupt input) of STM8S207S goes to...

huck by Associate II
  • 3680 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.