2014-10-21 2:25 AM
Hi,
I have problem with gpio interrupt. I am trying configure and enable interrupt by calling function GPIO_Init(GPIO0, GPIO_PIN_0, GPIO_MODE_IN_FL_IT) but without success. In interrupt handler function INTERRUPT_HANDLER(PORT2_IRQHandler,5) I am calling GPIO_WriteReverse(GPIO0, GPIO_PIN_2) and it is not working. When I put GPIO_WriteReverse(GPIO0, GPIO_PIN_2) in main loop, it works and PIN_2 is toggled. So I configured PIN_2 correctly. In STM8 I found EXTI_SetExtIntSensitivity(...) function. It has not representation in stlux library. Do you have any idea why INTERRUPT_HANDLER(PORT2_IRQHandler,5) not occur? How I must to do the correct configuration?2014-10-23 1:16 AM
Do you know where I can find example with external interrupt for stlux385a? I have some examples but they are not include external interrupt, only adc, comparators etc.
I tried use P2 port (digin) but I do not know where I can enable interrupt and where I can choose rising or falling edge. I do not find this information in datasheet. Please any help.2014-10-23 2:52 AM
I resolve my problem. Everything with port 2 interrupt are configurable by SMED configurator.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.