Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Viper28 voltage drop under load

Posted on May 07, 2015 at 19:14Hello I built a SMPS using the eDesignSuite. It is based on a Viper28, and was designed to output 15V 750mA from 80-265V AC. I wound my own transformer based on the specs from the design. Under no load the output is 14...

aquamoon by Associate
  • 3337 Views
  • 1 replies
  • 0 kudos

STM8S003k3 TIM1 PWM problem

Posted on May 08, 2015 at 15:44Hello every one. I have a workable code of pwm on STM8S105K4T6 and now I paste it in STM8S003k3 fnd it won't work.&sharpdefine CCR1_Val  ((u16)2047) // Configure channel 1 Pulse Width Blue&sharpdefine CCR2_Val  ((u16)2...

STVD: Preserve EEPROM

Posted on May 05, 2015 at 15:59How can I preserve the EEPROM contents when debugging my application on the STM8S003?I use STVD and either the STLink/V2 or the RLink.

STM8S003F3U programming

Posted on April 16, 2015 at 14:04I'm totally new to STM8 microcontroller series. I'm planning to do a project using STM8S003F3U controller in which ADC and timer module will be used. It would be useful if i could find some sample codes for ADC,timer...

what is eDesignStudio?

Posted on February 02, 2010 at 14:32eDesignStudio simplifies power supply design and offers to designers the flexibility to choose the right products and topologies.  A full design is generated from the high-level requirements specified by user and...

0690X00000603PXQAY.jpg
FDAMICO by ST Employee
  • 3428 Views
  • 6 replies
  • 0 kudos

Debugging problem of STM8

Posted on April 30, 2015 at 08:21I'm doing a project on STM8S003F3. Im using IAR instead of stvd for developmeant purpose. I could create my sample project and successfully debugged it. It was working fine for few days. But today debug session termi...

ST7580 USART with Arduino

Posted on February 01, 2013 at 06:02Hello,I'm having a problem interfacing my ST7580 using Arduino Mega USART. And I think I already broke 2 pcs of IC and I cannot afford to lose some more.Please help me code to PING, Read/Write MIB and send even si...

STM8 startup bug Timer 2 input capture

Posted on April 28, 2015 at 12:50 Hi, I wanna make a frequency pulse counter with an STM8. The counter is based on the input capture of the STM timer 2. The frequency is a frequency with a range of 1 Hz - 20 kHz. With the following ...

mitchell by Associate
  • 888 Views
  • 0 replies
  • 0 kudos

Bit Variables ISR Safe?

Posted on April 24, 2015 at 20:43I am using the Cosmic compiler and I want to read and write bit variables in an ISR.  I am wondering if there is a guarantee that ALL bit variable manipulations are atomic (ie using bitwise instructions).  If not - s...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.