Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CW half-bridge

Posted on September 25, 2014 at 09:53Why did you design a specific CW half-bridge with current limited in 0.6A output current capability? #ultrasound

sc by Associate
  • 1258 Views
  • 1 replies
  • 0 kudos

STHV748 THSD

Posted on April 17, 2015 at 10:59HiIs there any particular sequence of giving the THSD voltage? We initially had connected it to high voltage directly without giving the pull up resistor. The chip works fine when VDDM is given first and VDDP (also D...

arya by Associate
  • 1200 Views
  • 1 replies
  • 0 kudos

Resetting the beCAN error counters

Posted on April 20, 2015 at 14:28I'm in the process of implementing a CAN-based ad-hoc communication protocol on the STM8S208C8 MCU. Slave devices in this systems perform auto-baud detection by monitoring the receive error counter and trying the nex...

johanf by Associate
  • 1325 Views
  • 0 replies
  • 0 kudos

the reset output pin!

Posted on April 12, 2015 at 18:55we have adopted stm8 in our application and get into production a year ago, which seemed ok, in reasonablly sum of quantity.but recent two batch of chips, mainly stm8s208, also messed up with stm8s105, give us big he...

STM8S swim error 30100: can't load library

Posted on April 08, 2015 at 19:39I have a new STM8S-Discovery board. When conneting it to PC USB port and loading ''discovery'' project and using STVD to start debugging, I got this error message:  ** Connection error (usb://usb) [30100]: can't load...

STVD + Cosmic. Heap Size?

Posted on March 19, 2015 at 14:53Hello i am using STVD + Cosmic with stm8s105k4t6. And i have a problem. I need to allocate an array with 612 cells but:current_packet.data = (uint8_t*)malloc(current_packet.size+2);if (current_packet.data == 0)byteco...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.