2015-04-28 3:50 AM
Hi,
I wanna make a frequency pulse counter with an STM8. The counter is based on the input capture of the STM timer 2. The frequency is a frequency with a range of 1 Hz - 20 kHz. With the following code this is possible:
#include <
iostm8s003k3.h
>
#include <
intrinsics.h
>
#include <
stdio.h
>
#include ''stm8s.h''
unsigned int CaptureLow;
unsigned int CaptureHigh;
unsigned int CaptureValue;
unsigned int Freq;
unsigned char flag;
char string[20];
float Frequency;
//
// Setup the system clock to run at 16MHz using the internal oscillator.
//
void InitialiseSystemClock()
{
CLK_ICKR = 0; // Reset the Internal Clock Register.
CLK_ICKR_HSIEN = 1; // Enable the HSI.
CLK_ECKR = 0; // Disable the external clock.
while (CLK_ICKR_HSIRDY == 0); // Wait for the HSI to be ready for use.
CLK_CKDIVR = 0; // Ensure the clocks are running at full speed.
CLK_PCKENR1 = 0xff; // Enable all peripheral clocks.
CLK_PCKENR2 = 0xff; // Ditto.
CLK_CCOR = 0; // Turn off CCO.
CLK_HSITRIMR = 0; // Turn off any HSIU trimming.
CLK_SWIMCCR = 0; // Set SWIM to run at clock / 2.
CLK_SWR = 0xe1; // Use HSI as the clock source.
CLK_SWCR = 0; // Reset the clock switch control register.
CLK_SWCR_SWEN = 1; // Enable switching.
while (CLK_SWCR_SWBSY != 0); // Pause while the clock switch is busy.
}
void InitMCU(void)
{
PB_DDR = 0x0F;
PB_CR1 = 0x0F;
PB_ODR = 0x00;
PC_DDR_DDR1 = 1;
PC_CR1_C11 = 1;
PC_ODR_ODR1 = 0;
PC_DDR_DDR2 = 1;
PC_CR1_C12 = 1;
PC_ODR_ODR2 = 0;
}
void InitCaptureTIM2(void)
{
TIM2_PSCR = 3;
TIM2_CCMR1 = 0x01; //CAPTURE / VERGELIJK moderegister 1
TIM2_CCER1_CC1P = 0;
TIM2_CCER1_CC1E = 1;
TIM2_SR1_CC1IF = 0;
TIM2_SR2_CC1OF = 0;
TIM2_IER_CC1IE = 1;
}
void __delay(void)
{
unsigned long int j=200000;
while(j--);
}
//
// Setup the UART to run at 115200 baud, no parity, one stop bit, 8 data bits.
//
// Important: This relies upon the systemk clock being set to run at 16 MHz.
//
void InitialiseUART()
{
//
// Clear the Idle Line Detected bit in the status rerister by a read
// to the UART1_SR register followed by a Read to the UART1_DR register.
//
unsigned char tmp = UART1_SR;
tmp = UART1_DR;
//
// Reset the UART registers to the reset values.
//
UART1_CR1 = 0;
UART1_CR2 = 0;
UART1_CR4 = 0;
UART1_CR3 = 0;
UART1_CR5 = 0;
UART1_GTR = 0;
UART1_PSCR = 0;
//
// Now setup the port to 115200,n,8,1.
//
UART1_CR1_M = 0; // 8 Data bits.
UART1_CR1_PCEN = 0; // Disable parity.
UART1_CR3_STOP = 0; // 1 stop bit.
UART1_BRR2 = 0x0a; // Set the baud rate registers to 115200 baud
UART1_BRR1 = 0x08; // based upon a 16 MHz system clock.
//
// Disable the transmitter and receiver.
//
UART1_CR2_TEN = 0; // Disable transmit.
UART1_CR2_REN = 0; // Disable receive.
//
// Set the clock polarity, lock phase and last bit clock pulse.
//
UART1_CR3_CPOL = 1;
UART1_CR3_CPHA = 1;
UART1_CR3_LBCL = 1;
//
// Turn on the UART transmit, receive and the UART clock.
//
UART1_CR2_TEN = 1;
UART1_CR2_REN = 1;
UART1_CR3_CKEN = 1;
}
//
// Send the message in the string to UART1.
//
void UARTPrintF(char *message)
{
char *ch = message;
while (*ch)
{
UART1_DR = (unsigned char) *ch; // Put the next character into the data transmission register.
while (UART1_SR_TXE == 0); // Wait for transmission to complete.
ch++; // Grab the next character.
}
}
int main( void )
{
//Setup of program, initializing
__disable_interrupt();
InitMCU();
InitCaptureTIM2();
InitialiseSystemClock();
InitialiseUART();
__enable_interrupt();
TIM2_CR1_CEN = 1;
for(;;)
{
Frequency = (float)Freq/0;
sprintf(string,''%.2f \n\r'',Frequency);
UARTPrintF(string);
}
}
#pragma vector = TIM2_CAPCOM_CC1IF_vector
__interrupt void Timer2_CAPTURE_INT(void)
{
if(!flag)
{
TIM2_CNTRH = 0;
TIM2_CNTRL = 0;
flag ^= 1;
}
else
{
CaptureHigh = TIM2_CCR1H;
CaptureLow = TIM2_CCR1L;
CaptureValue = ((CaptureHigh << 8) | CaptureLow);
flag ^= 1;
Freq = 200000000/CaptureValue;
}
}
My problem is that there is a bug in the code. The timer UART output start always with a wrong frequency (1150 Hz), maybe a reset or an initialisation is wrong but I can't find the mistake?
When the frequency drops down, below 50 Hz, the system is working until a new system startup. With a new system startup there is the same start up problem.
What is wrong in my code??
Thankyou!!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.