Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8S003 vs STM8S103

Posted on May 18, 2016 at 16:00Hi Sir,Due to cost issue, I need to cost down from STM8S103 to STM8S003, could you kindly let me know what's different between these two part? Is there existing any known issue from STM8S003 that not written in lastly ...

STM8S Timer1 input capture issue

Posted on May 17, 2016 at 17:30Hello am working with the timer1 input capture of an STM8S103F3. No input is registered by the input capture module though I fed it with square waves from 10Hz all the way up to 1MHz. The same square wave registers pro...

jf by Associate
  • 880 Views
  • 0 replies
  • 0 kudos

Hello World

Posted on April 19, 2016 at 03:16Hello everybody. Can someone point me to a simple ''Hello world'' LED blinking example for STM8?My situation is as following:I found http://www.electroons.com/blog/stm8-tutorials-2-hello-world-program/ and I tried to...

d_aliaga by Associate II
  • 1612 Views
  • 2 replies
  • 0 kudos

STM8S207SB checksum fails with cosmic compiler

Posted on April 18, 2016 at 14:20Hi!I just tried to verify the FLASH according to CLASS B considerations. I followed the manual by using -ck for .text and -ik (.checksum area) flags for the linker,The descriptor is inside the s19 file, the map file ...

hjs by Associate II
  • 2445 Views
  • 3 replies
  • 0 kudos

VIPER 06L for 3.3VDC

Posted on April 13, 2016 at 19:13Hi, I am using the eDesign Suite to make a 3.3VDC Power Supply , but I am facing some problems .First of all , I got the schematic from the eDesign Suite and make it on Breadboard , It should has an output of 3.3VDC ...

0690X00000605dHQAQ.png

Source code for STEVAL-IAS003V1

Posted on April 19, 2016 at 07:45Hello,I amlooking for source code of ST STEVAL-IAS003V1 evaluation board board.UnfortunatelyI can not find in on ST web site and trough the Google to...Pleasehelp.Regards,Alex.

STM8 firmware library

Posted on April 14, 2016 at 09:32HelloI have been reading a document called Getting Started with the STM8 and they mentioned the ''STM8 firmware library''However I have spent a lot of time (really too much) trying to find this library. Searches insi...

d_aliaga by Associate II
  • 2850 Views
  • 4 replies
  • 0 kudos

ST7268x Production Tool

Posted on April 13, 2016 at 14:45Hi all , i need to re-configure  an old ST72681 fast usb flash controller . The problem is that i cannot find the tool needed to configure it . Does anybody know where this tool can be found ? Thanks in advance . L...

Big problem with STVD

Posted on April 05, 2016 at 12:15I have a workspace containing several projects; one of those projects has several building configurations. Randomly, the STVD switches the settings between the varoius configurations in this project, this way I am ne...

i2399 by Associate III
  • 1290 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.