2016-05-17 8:30 AM
Hello am working with the timer1 input capture of an STM8S103F3. No input is registered by the input capture module though I fed it with square waves from 10Hz all the way up to 1MHz. The same square wave registers properly in the input capture module of a pic micro. I have seen that the PC6 (TIM1 Channnel1) pin is set to TIM1 channel1 as an alternate function but I have not found anything helpful in the STM8S standard development library. I have pasted my code below in case anyone can help thanks:
#include ''stm8s.h'' void main() { CLK_DeInit(); CLK_HSICmd(ENABLE); CLK_LSICmd(DISABLE); CLK_HSECmd(DISABLE); CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1); CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV1); GPIO_Init(GPIOC, GPIO_PIN_4, GPIO_MODE_IN_FL_NO_IT); CLK_CCOConfig(CLK_OUTPUT_CPUDIV32); CLK_CCOCmd(ENABLE); GPIO_Init(GPIOC,GPIO_PIN_6,GPIO_MODE_IN_PU_NO_IT); TIM1_DeInit(); CLK_PeripheralClockConfig(CLK_PERIPHERAL_TIMER1 , ENABLE); TIM1_ICInit( TIM1_CHANNEL_1, TIM1_ICPOLARITY_RISING,TIM1_ICSELECTION_DIRECTTI,TIM1_ICPSC_DIV1, 0x00); TIM1_SelectInputTrigger(TIM1_TS_TI1FP1); TIM1_SelectSlaveMode(TIM1_SLAVEMODE_RESET); TIM1_ITConfig(TIM1_IT_CC1,ENABLE); TIM1_GenerateEvent(TIM1_EVENTSOURCE_CC1); TIM1_ClearFlag(TIM1_FLAG_CC1); TIM1_UpdateRequestConfig(TIM1_UPDATESOURCE_REGULAR); TIM1_Cmd(ENABLE); enableInterrupts(); while (1); } /***********Contents of stm8s_it.c*********************/ uint16_t Capture; uint8_t Buf[10]; INTERRUPT_HANDLER(TIM1_CAP_COM_IRQHandler, 12) { if(TIM1_GetITStatus(TIM1_IT_CC1)==SET) { Capture=TIM1_GetCapture1(); TIM1_ClearFlag(TIM1_IT_CC1); } }We’re moving the ST Community to a new platform to give you a better and more reliable community experience.