2016-04-18 5:20 AM
Hi!
I just tried to verify the FLASH according to CLASS B considerations. I followed the manual by using -ck for .text and -ik (.checksum area) flags for the linker,The descriptor is inside the s19 file, the map file shows 10 bytes as expected. My codesize is around 64k (I did not check lower sizes, but exceeding 64k boundary). I have to use the long stack model for my code.All _checksum/_checkCRC functions fail (result is not zero). I do not use breakpoints (I read the hint in one post), but it still does not work. The descriptor area starts at 0x18b96, code area at 0x9528-0x18b96.I tried Cosmic 4.3x and 4.4x (dongle license). No luck.What could be the reason for that?Best regards,HaJo2016-04-19 7:38 AM
HaJo
I had issues when first using the checksum routines. Turns out Cosmic had problems in some earlier versions of the compiler package. V4.3.12 or newer has these issues corrected. I am using ''ckcrc161()'' and it correctly (now) calculates the crcc in extended memory.jdf2016-04-19 9:05 AM
Hi John!
Are you using ckcrc161.s ''directly'' or _checkcrc16() (inside libisl.sm8, which should be the same)? By the way, _checkcrc16 crashes here, _checkcrc16x() does not crash. Could there be an issue with the libfiles or compiler flags (far library calls)? HaJo2016-04-21 5:00 AM
[SOLVED]
Fixed by cosmic support (updated linker)! 1. Descriptor section has to be in lower 64k area. So now my ''.cksum... -ik'' is in front of the other sections (.const and .text) at 0x8080, not behind .text. 2. It only works (in my case) with a modified linker. 3. The crashes were the result of the activated watchdog running out (in case of CRC16 check). Best regards, HaJoWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.