2016-11-21 4:34 AM
Hi everyone.
I have an .HEX file that I would like to program in a STM8AF62A8 MCU. I load the .HEX into STVP and it seems to be flashing the memory correctly because I can see some of the application's startup output through the serial port (it does it repeatedly due to the MCU being restarted multiple times during programming, I assume). The problem is that, as soon as the process is over, the MCU stops responding and I get no serial output when I reset the MCU manually. #hex #stvp #stm8Solved! Go to Solution.
2016-11-21 8:11 AM
Hello,
When STVP has finished, the Swim (communication) is disabled and the mcu is held under reset.
If you unplug the programmer, the mcu should be running.
Rgds,
Laurent
2016-11-21 8:11 AM
Hello,
When STVP has finished, the Swim (communication) is disabled and the mcu is held under reset.
If you unplug the programmer, the mcu should be running.
Rgds,
Laurent
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.