Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[ATT]9478

Posted on September 11, 2017 at 14:54TO Calculate PWM Duty Cycle Hello all,My question is regarding duty cycle vary according to ADC value I am using STM32F030R8T6 Controller TIM3 is used to generate 20khz signal Prescaler value is 47 and count peri...

STM8S001J3 I2C: Nothing happens

Posted on September 11, 2017 at 15:06 I'm trying to get I2C to work, but nothing happens on either SDA nor SCL. I've connected the STM8S001J3 like so: Pin 5 SDA Pin 6 SCL (There are pull-ups on both of the lines) 1. I initialize t...

Resolved! stm8l adc

Posted on August 31, 2017 at 09:46Hi guys, may some expert please help me? I am new to stm8l. I am currently using the chip stm8l151k4t6. I have connected battery voltage to pin D7, purpose of it is that i wanna monitor the status of the battery whi...

dion  tan by Associate II
  • 4177 Views
  • 6 replies
  • 0 kudos

I2C peripheral (STM8S005C6) not working

Posted on August 29, 2017 at 16:39*******************************I2C peripheral of STM8S005C6 not working******************************************I2C peripheral of STM8S005C6 does not jump to interrupt service routine:                  INTERRUPT_HA...

0690X000006083WQAQ.png 0690X000006083NQAQ.png

parameters of the transformer

Posted on August 20, 2017 at 16:20Himy name is pini i work on new project AC/DC converterthe input is 85-265 VACoutput  12vdc/350mAaxiliry :16vdcchip:viper013HSI work with a midcom transformer 750370024 and viper013hs I don't how to set this transfo...

Problem using Touch library with STM8S003K3.

Posted on September 01, 2017 at 20:30Hello all,I am using STM8S003K3 for my appplication with STVD IDE and Cosmic compiler and using Touch Library for my application.I have added touch library in project and configure it as to work with STM8S003K3.I...

P. S. by Associate
  • 823 Views
  • 0 replies
  • 0 kudos

Beep Function in STM8S003k3

Posted on September 30, 2015 at 05:06Dear AllI have a STM8S Discovery board. I want to config PD4 with Beep function./*Initialize PD4 for beep signal */GPIO_Init(GPIOD, GPIO_PIN_4, GPIO_MODE_OUT_PP_HIGH_FAST);BEEP_Init(BEEP_FREQUENCY_1KHZ);BEEP_Cmd(...

cv-chung by Associate
  • 1539 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.