Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STL140N4LLF5 Overcurrent - Marking Included

Currently, we have developed a USB HUB Board.When we manufactured 5EA for the first time, it worked normally. (Current: 50mA)When we manufactured 10EA for the second time, 5EA worked normally, and 5EA had overcurrent. (Overcurrent: 450mA)After analyz...

Kang1_0-1750122349599.png
Kang1 by Associate II
  • 716 Views
  • 1 replies
  • 1 kudos

Possible counterfeit: TSD4M250AV

Hi everybody!I´m repairing a big ClassD amplifier from the 90s and I needed to replace four old TSD4M250V mosfet isotop modules. I tried with modern parts (IXFN140N20P from IXYS), without fails or smoke troubles, but they not working correctly (the c...

`stmmac` driver error: MAC to MAC communication

Hi there,I am trying to use the stmmac driver the .dtsi here to connect two GMII MAC components.gmac0 and gmac1 are activated as followed in a separate .dts file - note that gmac2 is configured and confirmed to be working prior to this:&gmac0 { stat...

K606 by Associate
  • 918 Views
  • 2 replies
  • 1 kudos

Resolved! ECMF02-4CMX8 operating temperature

Hello, My system is required to operate at -40C.The datasheet states that low range ambient temperature is -30C, while the junction temperature is -40C.Can you please explain the discrepancy between the two? Under what conditions can the junction tem...

Alex_Kucherov_0-1749408500626.png

Resolved! STM8S103 Timer TIM2 timing

Hi,Using ST Workbench debugger my 16-bit timer TIM2 (china bought) overflows each 16 seconds as the prescaler is set to 10. With an 16MHz internal clock divided by 2^10 (1024) the timer should overflow theoretically each 4.1 seconds. Prescaler 9 take...

sthvw by Associate III
  • 2619 Views
  • 9 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.