2025-06-08 11:49 AM
Hello,
My system is required to operate at -40C.
The datasheet states that low range ambient temperature is -30C, while the junction temperature is -40C.
Can you please explain the discrepancy between the two? Under what conditions can the junction temperature be lower than the ambient temperature?
Can I use the ECMF02-4CMX8 in my case?
Thank you in advance.
Solved! Go to Solution.
2025-06-11 12:10 AM
Hello,
The ECMF02-4CMX8 can be used at -40°C.
Datasheet will be modified with Top between -40°C and +85°C.
Best regards.
Fabrice.
2025-06-09 6:03 AM
> Can I use the ECMF02-4CMX8 in my case?
> My system is required to operate at -40C.
> The datasheet states that low range ambient temperature is -30C
If you want to remain within the allowable limits of the datasheet, no this doesn't work. It's a bit odd, but that's what the DS says and we have no reason to distrust it. It's also on rev 4.
2025-06-10 2:13 PM
Hi TDK,
It would still be helpful to understand the reason for the -30C limit, since as you mentioned, it is a bit odd.
Does the -40C junction temperature refer to the TVS diodes while the -30C is limited by the common mode filter?
2025-06-11 12:10 AM
Hello,
The ECMF02-4CMX8 can be used at -40°C.
Datasheet will be modified with Top between -40°C and +85°C.
Best regards.
Fabrice.
2025-06-23 12:45 AM
Good morning, my name is Arnaud Fardoit, I'm product marketing engineer in charge of filtering/protectino products for US region. We have been informed that our ECMF02-4CMX8 is going to be phase out very soon and not recommended for new design anymore. We recommend our ECMF2-40A100N6 for datalines, our ESDA17P20-1F2 for VBUS line and ESDZV5H-1BU2 for ID line. My colleague Fabrice has been informed about the change, sorry for the inconvenienced caused. Best Regards, Arnaud
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.