2025-05-07 5:33 AM
Hello All,
We planned to use STM Airbag IC- L9678P-S for one of our automotive application development. We intended to use L9678P-S having PSI5 /SPI/I2C sensor interface using Evaluation Board set up . Can some one share the Schematic of the EVB L9678P-S board .
Thanks in advance.
Regards
Sharma
Solved! Go to Solution.
2025-05-07 6:13 AM
Welcome @Sharma, to the community!
The L9678P-S is an automotive device whose tools and full documentation are usually only available from your local distributor or STMicroelectronics office.
Hope that helps?
Regards
/Peter
2025-05-07 6:13 AM
Welcome @Sharma, to the community!
The L9678P-S is an automotive device whose tools and full documentation are usually only available from your local distributor or STMicroelectronics office.
Hope that helps?
Regards
/Peter
2025-05-07 7:18 AM
Hello Peter,
Appreciate your quick response on my query. I am located in Bangalore/India. Is there a possibility for you to provide ST Bangalore/India contact email ID for me to get connected and avail their help .
2025-05-07 9:06 AM
All contact details can be found with the URL if you select the contact type and your region:
https://www.st.com/content/st_com/en/contact-us.html
2025-06-25 5:59 AM - edited 2025-06-25 6:12 AM
Hello Peter,
We received the L9678P EVB schematic from the distributor and working on building an application for air bag system.
At the beginning, we are trying to make the EVB up running for the SPI/PSI5 communication. In our set up, we had connected ADI chip set (processor-master ) to SBC L9678P-S for SPI communication at 5 Mhz clock. VDDQ supply is set to VDD3V3 since the micro operates at 3.3V.
We could able to establish the SPI communication between ADI chip set (processor-master ) and L9678P-s(Slave). We were able to set/turn on the power supply pins on L9678P-s like ERBOOST(33v), VSUP(6.8V). by sending the following SPI write messages.
Input supply voltage VBat = 12V , Watchdog Enabled and VRESdiag jumper on the EVB set to VRBOOST.
Here are the SPI messages we are sending from ADI chip set to L9678P-S in enabling the power supplies:
SPI Register address $01 SYS_CFG SPI Message : 00 02 55 ED
SPI Register address $02 SYS_CTL SPI Message : 00 05 1E E0
After sending the above SPI messages, L9678P is able to set the ERBOOST voltage to 33V and VSUP to 6.8Volts. After this step, we are trying to enable PSI5 communication on channel 0 by turning ON the RSU0 supply by sending the following SPI messages.
SPI Register address $4A RSCR1 SPI Message : 00 94 00 00
SPI Register address $4E RSCTRL SPI Message : 00 9C 00 02
After sending above SPI messages, we tried to measure the voltage at RSU0 terminal using multimeter and it always shows 0 volts ( P.N : PSI5 sensor is connected between RSU0 and GND ). Looks like the PSI5 channel0 power supply controlled through register RSCTRL bit 1 - CH0EN is not getting enabled/set. Can you please help us out in resolving the RSU0 power supply issue for PSI5 axis accelerometer sensor interface.
Thanks in advance
Regards
Sharma.
2025-06-25 7:21 AM
Your first question was about the documentation for this device, but my answer also refers to the support for it. If you have any questions, please contact the local distributor again, or alternatively the personal online support OLS.
Regards
/Peter
2025-06-25 10:41 PM
Hello Peter,
Thanks for your input. Sorry to say that ST local support is very very minimal or No. Hence we need further technical support in resolving the issue. As you indicated in the email I will post my query in OLS - ST.
Regards
Sharma
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.