Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Hello! I'm learning to code an STMicroelectronics 8 bit micro-controller. I want to control a BLDC motor with this MCU for electric vehicle application. I'm using the STM8S DISCOVERY Board, based on the STM8S105C6T6 (48 pin) MCU. This MCU has 4 timer...
Hi.I have faced a weird problem using IAR compilers.Errorstatus=0; Relay_Off; delay_ms(200); if(Errorstatus==1){ Errorflag=1;In this part of my code after I switch the relay off, I put a delay and if an interrupt...
I have Nucleo-L152RE board and I used this board to program the STM32 MCU using JTAG (CN4) connector. Now, I want to program the STM8 board using SWIM interface. So, is it possible with Nucleo-L152RE?. I already done the required changes to use Nucle...
When I develop the digital communication board using the ST10F269, I see the problem.- Problem: Although the interrupt signal is normal, interrupt handler of ST10F269Z2T3 is not working.I want to receive the advice about this problem.Q1) What is the ...
Can you also confirm how many pins have inbuilt ESD diode? According to datasheet its 2. But according to diagram in datasheet 4 pins have ESD.Also suggest which choke is better for USB 2.0 and USB 3.0 application among these two.ECMF02-2HSMX6 or ECM...
float get_resi(void) in https://gist.github.com/goog/bf784c5f63a199ddbde7cd49db92f73fcould you help to check the get_resi function?im not sure whether my time counter has some issue?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.