Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Thank you for allowing me to join. I am looking for technical data for a Thyristor, Particularly the operating temperature of the device.

The details on the device are ST DS(5)NM6 0(O) 6K0(O)8H222 I have indicated in brackets the option for the read symbols on the device as I may have misread them. This device is fitted in a Carlo Gavazzi DMB01C timing relay and it appears to ...

MWalt.8 by Associate
  • 1047 Views
  • 1 replies
  • 0 kudos

Normal files needed to use STM8 with STVD and Cosmic

I am working on my first STM8 project and getting used to its own flavour of quirks etc.Setting up a new project installs stm8s_interrupt_vector.c which I understand. I want to use the standard peripheral drivers so have downloaded them and added the...

BCowa by Associate II
  • 1009 Views
  • 0 replies
  • 0 kudos

timer code

static void TIM1_Config(void) { CLK_PeripheralClockConfig(CLK_Peripheral_TIM1, ENABLE); TIM1_DeInit(); // 2m/ 40 TIM1_TimeBaseInit(39, TIM1_CounterMode_Down, 0xffff, 0); //timer freq = (clock CPU/16) -> 1bit = 1uS -> 92...

how to disable RX interrupt temporarily

#if I2C_ENABLE USART_ClearITPendingBit(USART1, USART_IT_RXNE); USART_ITConfig(USART1, USART_IT_RXNE, DISABLE); p_write = (uint8_t *)&temp100; sEE_WriteBuffer(p_write, write_addr, 2); USART_ITConfig(USART1, USART_IT_RXNE, ENABLE); printf("i2c write do...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.