2019-08-23 2:13 AM
2019-08-23 4:26 AM
ECMF02-2HSMX6 can also be used for USB 2.0. On datasheet, fig 13 and 14 give USB 2.0 eye diagram with and without part, to show that it is OK for USB 2.0, and to show that impact on eye diagram is very low.
2019-08-24 2:48 AM
2019-08-24 6:38 AM
2019-08-27 12:23 AM
Hi,
ECMF02-2AMX6 is dedicated to USB 2.0, and it was not tested for USB 3.0.
For USB 3.0, we recommend:
For USB 2.0 and USB 3.0, I recommend ECMF02-2HSMX6.
Regards.
Fabrice G
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.