Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8 SPI slave device data read

Hi,I want to read more than one byte of data from slave device. I am using STM8AF family micrcontroller in master mode and pressure sensor SMP580 is a slave device. Master will send command which is of 1-byte to read 16 bit data from slave device. An...

DOman.1 by Associate II
  • 983 Views
  • 0 replies
  • 0 kudos

ADC request DMA transfer

Hello,we are using STR73x device. Our application needs to get 1 ADC sample every 5 ms and uses DMA to transfer that to memory.to do this, we setup a TB1 timer to trigger every 5 ms.On TB1 interrupt, we start a single shot ADC conversion.This works ...

HNguy.1 by Associate
  • 924 Views
  • 0 replies
  • 0 kudos

How protect GPIOs from ISO7637-3 Pulses?

Hi,I would like to protect my GPIOs from ISO7637-3 pulses with a rail to rail diode solution. But I have seen that the GPIOs already have a intern rail to rail protection with a forward voltage Vf_int = 0.6V (Datasheet Fig. 43). To protect my GPIOs w...

TLich.1 by Associate
  • 1578 Views
  • 2 replies
  • 0 kudos

I am using MC peripheral part# ZPSD301B-90JI in one of my applications. This part is obsolete and no longer supported by ST. I want to know if I can get any information on how to program a fresh MC. Can I do it with PSDsoft? What hardware is needed

I have BK Precision 864 universal programmer. Can I use it to flash this MC? Or please let me know what hardware (cables, prorammer hardware etc) is needed if I use PSDSoft software.

HSain.1 by Associate
  • 774 Views
  • 0 replies
  • 0 kudos

SPWF01SC UART not responding

We have used Wifi Module “SPWF01SC�? in one of our projects. Now recently we are getting more issue in wifi module.Most of the modules are not responding to AT commands. Can you please suggest possible troubleshoot steps to resolve this issue.

VShri.1 by Associate
  • 1091 Views
  • 1 replies
  • 0 kudos

wifi who wants not connected

Hello,I want to connect esp8266 wifi using stm32f4 to an access point, I find that the module is not stable; sometimes it connects and sometimes no, I didn't understand why. can someone gone through that please help me?here is my code and thanks in a...

MHMallek by Associate II
  • 730 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.