2019-12-18 3:26 AM
Hi,
I would like to protect my GPIOs from ISO7637-3 pulses with a rail to rail diode solution. But I have seen that the GPIOs already have a intern rail to rail protection with a forward voltage Vf_int = 0.6V (Datasheet Fig. 43). To protect my GPIOs with a extern circuitry the Vf_ext has to be lower than Vf_int, is that right?
Kind regards
Tom
2019-12-18 7:07 AM
Normally it's only around 0.3 V the forward voltage drop on the port reverse diodes. What datasheet do you have with 0.6 V?
2020-01-07 9:54 AM
I got the Information from this data sheet (p.85 fig.43): https://www.st.com/resource/en/datasheet/stm8af52a8.pdf
Where can I find the information of a forward voltage of 0.3V?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.