2020-01-03 7:12 AM
Hi,
I want to read more than one byte of data from slave device. I am using STM8AF family micrcontroller in master mode and pressure sensor is a slave device. Master will send command which is of 1-byte to read data from slave device. And slave will respond 2-bytes of data. So while sending command do i need to send command of 2-byte ?
2020-01-03 8:32 AM
Because telepathic support is yet to be deployed, help the humble mortals by telling which pressure sensor we are talking about, and if it is 3 or 4 wire SPI.
2020-01-05 11:04 PM
I am using SMP580 pressure sensor.
It is 4 wire spi (MOSI,MISO,CLK,CS). If i send only 1 byte command does the slave will send responce of 2byte ?
2020-01-07 6:30 AM
any suggestions ??
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.