2020-01-06 12:28 PM
Hello,
I want to connect esp8266 wifi using stm32f4 to an access point, I find that the module is not stable; sometimes it connects and sometimes no, I didn't understand why. can someone gone through that please help me?
here is my code and thanks in advance.
void connect_wifi(){
uint8_t state=0;
//restore "AT+RESTORE\r\n"
Transmit_uart("AT+RESTORE\r\n");
HAL_Delay(100);
switch(state){
case 0:
//MODE
Transmit_uart("AT+UART_DEF=115200,8,1,0,0\r\n");
HAL_Delay(100);
Transmit_uart("AT+CWMOD=1\r\n");
HAL_Delay(100);
state++;
case 1:
//acces point
Transmit_uart("AT+CWJAP=\"p9\",\"azaz1212\"\r\n");
HAL_Delay(5000);
state++;
case 2:
//get ip
Transmit_uart("AT+CIFSR\r\n");
HAL_Delay(100);
break;
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.