Is there any PS/2 keyboard/mouse library available?
Is there any working PS/2 keyboard/mouse library available for STM8 microcontroller?Best Regards,tinkerBOY
Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.
Is there any working PS/2 keyboard/mouse library available for STM8 microcontroller?Best Regards,tinkerBOY
Hi,I have a weird issue !I am developing an application where i Use the M24C64-WDW6TP EEPROM.First I need to be sure, this eeprom have 8KB of memory, every page is 32B so it has 256 pages.is the page address = (page number - 1 )*page_size ?? for exam...
I am using standard peripheral library for STLUX and using stm8 library for I2c interface. I have tried with all the examples in libraries which are using interrupt handlers. Also, i have tried the online examples for stm8 using poll methods. Nothing...
Hi,I have STM32WB55RG and GNSS1A1 boards. I am trying to run SimOSGetPos example however my GNSS1A1 module returns only empty messages. As far as I was able to troubleshoot, I found function GNSS_PARSER_ParseMsg which enters infinite loop that is loo...
Hi allwe are using a custom PCB with the STHV800 IC on it, in the past we've used it primarily as a pulser IC, not yet to take the reading signal into account. Now that we want to take a look at the echo, we don't see the expected echo when comparing...
"M27C256B-10F1"�?�該�?�判定書を頂�?�る�?��?�ょ�?��?�。購入先�?�商社�?�廃業�?��?��?��?��?�り�?購入実勢�?��?��?�商社�?��?��?該�?�判定書�?�発行を対応�?��?�もら�?��?��?�ん。宜�?��??�?�願�?��?��?��?��?��?�。
The EEPROM M95512-D has an identification page that could be write protected permanently. In teh datashett is the address of this page not mentioned. I need to know the address for the identification page.
I was making a basic test for GPIO ports (reading switches and turning on LEDs). After configuring PORTB (all pins) as input with internal pull-up and external interrupts disabled, PB7 seems to be always in '0'. After opening IAR-EW debugger, PB_DDR...
We are using STM8 as to monitor and control STMF07 controller and Quectel M66 module if they are not sending pulses in predetermined time. But no physical control or method to reset STM8, So can we restart the program control of STM8 through softwar...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.