Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MCU Proposal

I am looking for STM32 series product for my Automotive Meter customer.Required spec: 16KB/2KB, 16MHz, 2.7V to 5.5V, VQFN, -40°C to +125°C Application: Automotive meterI checked below ST link, and it seems that below links are OK (?) to meet above re...

PLaw.1 by Associate
  • 1775 Views
  • 4 replies
  • 0 kudos

B-L475E-IOT01A - TCP Server Library (AT Commands)

Hi,​I recently started using this board (​B-L475E-IOT01A) which has a WiFi module that uses AT Commands.​I have been using some libraries provided by Mbed website, but none of them have a TCP Server socket implemented, just a client.​​I tried to do i...

LModd by Associate
  • 1324 Views
  • 2 replies
  • 0 kudos

LDP01-35AY ISO16750-2 pulse

Dear sir or madam,we are using the LDP01-35AY twice in our design for input protection as given in ISO 7637-2 and ISO 16750-2. Unfortunately the load dump pulse destroys our input circuit. I did an extrapolation of the "Safe Operation Mode" of the di...

Mvon .1 by Associate II
  • 4145 Views
  • 4 replies
  • 0 kudos

WiFi

Hi,can someone givee the link of a reference manual or sthg like that showing how to use every single API of the WiFi)thank you

idrissmc by Associate III
  • 745 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.