2020-03-01 6:21 AM
Is there any working PS/2 keyboard/mouse library available for STM8 microcontroller?
Best Regards,
2020-03-21 6:44 PM
I found a possible PS2 keyboard implementation for the STM8 mcu using this. I tried compiling on STVD but i keep getting errors.
----------- Project ps2_keyboard - STM8 Cosmic - Configuration Debug -------------
Compiling ps2_keyboard\main.c...
cxstm8 -iinc -ips2_keyboard +debug -pxp -no -l +mods0 -pp -i"C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Hstm8" -clDebug\ -coDebug\ ps2_keyboard\main.c
#error cpstm8 C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Hstm8\stdint.h:9(20+6) redeclared typedef int8_t
#error cpstm8 C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Hstm8\stdint.h:10(21+7) redeclared typedef int16_t
#error cpstm8 C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Hstm8\stdint.h:11(20+7) redeclared typedef int32_t
#error cpstm8 C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Hstm8\stdint.h:12(22+7) redeclared typedef uint8_t
#error cpstm8 C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Hstm8\stdint.h:13(23+8) redeclared typedef uint16_t
#error cpstm8 C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Hstm8\stdint.h:14(22+8) redeclared typedef uint32_t
#error cpstm8 ps2_keyboard\main.c:26(17) redeclared external putchar
#error cpstm8 ps2_keyboard\main.c:135(0) missing enumeration member
#error cpstm8 ps2_keyboard\main.c:349(0) missing enumeration member
#error cpstm8 ps2_keyboard\main.c:355(0) missing enumeration member
#error cpstm8 ps2_keyboard\main.c:447(20) missing prototype
#error cpstm8 ps2_keyboard\main.c:471(23) missing prototype
#error cpstm8 ps2_keyboard\main.c:488(13) missing prototype
#error cpstm8 ps2_keyboard\main.c:515(19) missing prototype
#error cpstm8 ps2_keyboard\main.c:524(26) missing prototype
#error cpstm8 ps2_keyboard\main.c:513(24+8) __func__ undefined
ps2_keyboard\main.c:
The command: "cxstm8 -iinc -ips2_keyboard +debug -pxp -no -l +mods0 -pp -i"C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Hstm8" -clDebug\ -coDebug\ ps2_keyboard\main.c " has failed, the returned value is: 1
exit code=1.
main.o - 18 error(s), 0 warning(s)Any idea?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.