Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Writing data to M95M04

I am creating a program to write data arbitrarily to the M95M04. The M95M04 has 512-byte pages, but does writing have to be done in page units?For example, when writing 8 bytes of data starting from address 8, is it acceptable to specify address 8H a...

totaw.1 by Associate II
  • 446 Views
  • 2 replies
  • 0 kudos

Resolved! STHV200 Amplifier Feature

Hi,I am trying to understand some features of STHV200 Dual channel ±100 V, high voltage 3 A linear amplifier and 2 A pulser transmitter.I could not find a detailed datasheet of the product. Only data brief. I want to use it to amplify the received lo...

Stm325 by Associate III
  • 593 Views
  • 2 replies
  • 3 kudos

Resolved! Material declaration report for M93C86-WMN6P

Our customer has requested a material declaration report for M93C86-WMN6P. We purchased 1,000 pcs from Avnet back in 2016. However, it appears that this part is now inactive, as I couldn’t find the part number listed under M93C86-W. Could you kindly ...

STI by Associate II
  • 346 Views
  • 1 replies
  • 1 kudos

STM32 Blue Pill CAN Issues

The board has passed a authentication test so I currently believe it is a me issue. I have been trying to get a CAN bus going using the STM32 Blue Pill board with a TJA1050 CAN Transceiver, but for some reason even with basically copy pasted example ...

RetroBuzz by Associate II
  • 3134 Views
  • 18 replies
  • 2 kudos

Resolved! End of Life status for EMIF06-MSD02N16

We are currently evaluating components for a new product design and are considering the following ST part:Part Numbers:EMIF06-MSD02N16Before proceeding, we would like to confirm the lifecycle status of these components. Specifically, we would appreci...

rikpat by Associate II
  • 703 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.