Others: hardware and software

Discuss hardware and software design challenges, including NOR flash storage, OTA updates, component ID, and thermal management.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8L051F3P6 Power-up grey zone

I'm finding a window between 1.47V and 1.5V where the device is consuming 1mA (as opposed to <50uA) this is only apparent when the voltage is rising and I assume the device trying to power on. The documentation states it has zero power on reset but t...

Plum by Associate II
  • 1172 Views
  • 0 replies
  • 0 kudos

I use the software SmartGrid LabTool to develop ST8500, Auto Detect gets the result No feedback from Target, is there any way to solve it?

ST8500 is developed using the software SmartGrid LabTool, and the result of Auto Detect is No feedback from TargetIs there any solution?current test planReplace another port (port checked)Install other versions of cp2105 to serial driverEnvironment: ...

0693W00000Y6xdPQAR.png
DZhu.1 by Associate
  • 1108 Views
  • 0 replies
  • 0 kudos

Resolved! What happen if make write data to "ST EEPROM IC M24C64-F" the same address more than 4 million write cycles (spec)?

Hello: I have a ST EEPROM IC type is "M24C64-F". If I try make write data to the same address over than spec write cycles(4million) , so, does it affect other address's retention data? Does it only affect the data of the address that is written repea...

IdeaSTM8 - all source files turned red in Fileview/Source Files list. Can no longer compile. Any idea on what I need to fix?

I have used IdeaSTM8 for 3+ years with great success ... but this morning my project wouldn't compile, appearing to indicate that all functions were undefined. The only anomaly I see is that the Fileview / Source Files list has turned all my .c files...

0693W00000WLYqfQAH.png
MNiel.2 by Associate
  • 941 Views
  • 0 replies
  • 0 kudos

Teseo-LIV3F : NMEA messages

I am facing problem Teseo-LIV3F is not sending out any NMEA messages and also not accept any commands. Anyone know Why? and How to set back to "Factory Setting" ?

KSamn.1 by Associate
  • 2130 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.