2022-12-28 1:09 AM
I am using a NUCLEO-S8208RB to develop UART1 communication in half-duplex, single-wire mode. The device receives messages (packets of bytes) using the UART1_IT_RXNE_OR interrupt. The next step would be to transmit a byte packet in response, without an interrupt. That does not work. I suspect the UART1_TX configuration is wrong.
* IDE: STVD with COSMIC compiler and STVP.
* STM8 Standard Peripheral Library.
UART1 configuration code (this works):
UART1_DeInit();
UART1_Init((uint32_t)UART1_BAUDRATE, UART1_WORDLENGTH, UART1_STOPBITS, UART1_PARITY, UART1_SYNCMODE, UART1_MODE_TXRX_ENABLE);
UART1_ITConfig(UART1_IT_RXNE_OR, ENABLE);
UART1_HalfDuplexCmd(ENABLE);
enableInterrupts();The UART1_RX interrupt call function uses this code snippets:
void UART1_RX_Handler_Callback()
{
uart1RxData_u8 = UART1_ReceiveData8();
...
UART1_ITConfig(UART1_IT_RXNE_OR, DISABLE);
}The following code for UART1_TX does not work. It 'hangs', likely due to wrong UART1 register settings. Please comment. Thank you!
void UART1_TransmitPacket8()
{
uint8_t nBytesToSend = (uint8_t) PACKET_MAX_LEN;
TxCounter1 = (uint8_t) 0;
while (nBytesToSend > 0)
{
while (UART1_GetFlagStatus(UART1_FLAG_TXE) == RESET)
{ }
UART1_SendData8(uart1_TxBuffer_u8[TxCounter1]);
nBytesToSend--;
TxCounter1++;
}
while (UART1_GetFlagStatus(UART1_FLAG_TC) == RESET)
{ }
}
2022-12-28 6:55 AM
UART1_SYNCMODE?
Mode should be asynchronous.
2022-12-28 11:07 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.