2022-12-29 11:31 AM
I'm finding a window between 1.47V and 1.5V where the device is consuming 1mA (as opposed to <50uA) this is only apparent when the voltage is rising and I assume the device trying to power on. The documentation states it has zero power on reset but this behavior doesn't seem to match.
I also found this paragraph which I thought was related
When the BOR is disabled, a "grey zone" exists between the minimum operating voltage
(1.65 V)(a) and the VPOR/VPDR threshold. This means that VDD can be lower than 1.65 V
without device reset until the VPDR threshold is reached. For more details concerning the
power on/power down reset threshold, refer to the electrical characteristics of the datasheet
but the footnote states: "Not applicable on STM8L05xx value line devices. Refer to datasheets for more details" Which is what I have so now I'm not sure.
I'm just looking for a way to prevent this spike in power consumption, I tried enabling the BOR_ON bit in the options but it made no difference.
Do I have to resort to external circuitry or is there a way to prevent this via the chip configuration?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.